Primary States (Sideloop PI With Reset Staged Output) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
  • Off: Set the Percent Cmd to 0%.

  • Max: Set the Percent Cmd to 100%.

  • Control: Adjust the Percent Cmd to control the Process Variable. If the Process Variable is reliable, the module controls the Percent Cmd in order to maintain the process variable at the Setpoint. The Setpoint is reset based on the Reset Input and the limits Reset A, Reset B, Setpoint A, Setpoint B.