Reliability (Sideloop PI with Reset Proportional Output) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
Table 1. Sideloop PI With Reset Proportional Output Reliability

Input

Behavior When Input Is Not Reliable

Process Variable

If the State is Control, the PID skips execution and holds its output at its last value.

Reset Input

The last Reliable value is used as the input.