Primary States (Sideloop Interlock Binary to Binary) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
  • Off: The Present Value is set to Off.

  • On: The Present Value is set to On.

  • Control: If the Input is On and all timers are satisfied, the Present Value is set to On. If the input is Off and all timers are satisfied, the Present Value is set to Off.