The following table describes the attributes used by the Sideloop Interlock Binary to Binary module.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Input |
Contains input to this module. |
Off Set Name: Off/On |
|
|
Mode |
Contains the connection to the Selection object of a control System. It overrides the internal logic. |
Control Set Name: Off/On/Control |
|
|
Present Value |
G, V |
Contains the output based on the input and the status of the associated delays. |
Set Name: Off/On |
|
SL-DELAYTYPE (Delay Type) |
Selects the type of delay from the time the binary input is energized or de-energized to the time when the analog output goes to Output Range High or Output Range Low. This can be set to None, On, Off, or Both. |
None Set Name: BI to BO/AO Delay Type |
|
|
SL-OFFDELAY (Off Delay) |
Selects the delay from the time the input is de-energized to the analog output going to the Output Range Low. |
30 Seconds |
|
|
SL-ONDELAY (On Delay) |
Selects the delay from time the binary input is energized to time when the analog output goes to Output Range High |
30 Seconds |