Global Sequencer Miscellaneous Configuration - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

See Global Sequencer for more information.

Table 1. Attributes for Miscellaneous Configuration
Name Description Mode
Instant Shutdown Delay This delay value is used by the Instant Shutdown feature to control the rate at which the devices turn off. SP, SQ, ER, BC, ES
Inter-stage Delay On Rotate This Boolean value indicates whether or not Minimum On/Off and Inter-stage On and Off timers must be respected before a rotation can occur (from either the Rotate command or the Rotate Now input). When the property is False, the primitive ignores any of these timers and proceeds with the rotation. When this property is True, the primitive ignores the Rotate Now Delay, but does respect it when the property is False.

This attribute is available when you select Inter-stage.

ER, BC, ES
Oil Pump Off Delay This delay value is used by the Oil Pump feature to determine how long to run the oil after stopping the last compressor. This is an optional item typically used with chillers.

This attribute is available when Oil Pump on Device 1 is False.

SP, SQ, ER, ES
Oil Pump On Delay This delay value is used by the Oil Pump feature to determine how long to run the oil before starting a compressor. This is an optional item typically used with chillers.

This attribute is available when Oil Pump on Device 1 is False.

SP, SQ, ER, ES
Oil Pump On Device 1 This property indicates whether the single oil pump runs with the compressor attached to Device 1 Out or has its own motor. This is an optional item typically used with chillers. SP, SQ, ER, ES
Pump Down Available This property indicates whether a solenoid valve is connected to the Solenoid Valve output and a Low Pressure input is connected to the low pressure input. When this input is True, the stager provides a pump down using the low pressure input and solenoid valve output. This is an optional item typically used with chillers. SP, SQ, ER, ES
Rotate Now Delay

This delay value is used by the Rotate Now feature to turn new devices on before turning previously running devices off.

This attribute is available when Inter-stage Delay On Rotate is False.

ER, BC, ES
Time Remaining Update Interval This property controls how fast the Time Remaining outputs update. If this value is zero, the Time Remaining output does not update. This is used to conserve system bandwidth if no timer diagnostics information is needed. SP, SQ, ER, BC, ES
1 SP = Step, SQ = Sequential, ER = Equal Runtime, BC = Binary Code, ES = Equal Startup