Reliability (Zone Damper w Proportional Heating Valve) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Table 1. Zone Damper w Proportional Heating Valve Reliability

Input

Behavior When Input Is Not Reliable

Process Variable

Damper action set based on the Unreliable Option input.