Attributes (Motor Protection) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The following table describes the attributes used by the Motor Protection modules.

Table 1. Motor Protection Attributes

Name

Type 1

Description

Default Value

Blocking On Time

 

Indicates the amount of time that the motor is turned on when blocking protection is required.

5 seconds

Max Off Time

 

Indicates the maximum amount of time that the motor can be off before this module starts the motor for the Blocking On Time.

7.0 days

Motor Input

 

Current requested command to the motor.

Off

Set Name: Off/On

Motor Output

G

Provides the final output to the motor.

Off

Set Name: Off/On

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)