Blocking Protection - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Motor Protection module monitors the output command for a motor. If the command is off for an extended period of time, the motor starts for a short amount of time.

You can view or modify the modules in this group’s logic.