Module Use in Applications (Staged Box Heating Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Heating Staged Outputs with Low Limit Uses in Application System Selection Trees

Module Instance Name

Applications

Staged Box Heating Control v50

VAV Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.