The following table describes the attributes used by the HeatingCooling Valves w Shared AO modules.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Cooling Control Status |
Indicates current status of the controller for cooling control. |
Overridden Set Name: Control Status |
|
|
Cooling isAvailable |
Indicates cooling can be use to maintain support. |
True |
|
|
Cooling Mode |
Indicates the desired mode of operation for the cooling operation. |
Off Set Name: COM Valve Out |
|
|
Cooling Percent Cmd |
Indicates cooling percent. |
0% |
|
|
Cooling Position |
Provides the current Present Value of the output that this controller drives |
0% |
|
|
Cooling Setpoint |
Indicates desired setpoint to which the process variable is controlled to when commanded to Control Cooling. |
23 °C, 74 °F |
|
|
Failsoft Cooling Value |
Indicates the value of the output when commanded to control cooling and the process variable is unreliable. |
0% |
|
|
Failsoft Heating Value |
Indicates the value of the output when commanded to control heating and the process variable is unreliable |
0% |
|
|
Flush Position |
Indicates the percent heating or cooling that is commanded according to the flush mode setting (heating or cooling). |
100% |
|
|
Heating Control Status |
Indicates the current status of the controller for heating control. |
Overridden Set Name: Control Status |
|
|
Heating isAvailable |
Indicates heating can be use to maintain support |
True |
|
|
Heating Mode |
Indicates the desired mode of operation for the heating operation. |
Off Set Name: COM Valve Out |
|
|
Heating Percent Cmd |
Percent Heating requested. |
0% |
|
|
Heating Position |
Provides the current Present Value of the output that this controller drives. |
100.0% |
|
|
Heating Setpoint |
Indicates desired setpoint to which the process variable is controlled to when commanded to Control Heating. |
21 °C, 70 °F |
|
|
Limited Max Value |
When commanded to Limited Max Heating or Cooling, the output is restricted to this value. |
100% |
|
|
LowHigh Range Select |
Specifies which control is handled by the lower half of the analog output range (effectively 50% to 0%) |
HeatingCooling Set Name: FC 4-Pipe Range Select |
|
|
Output Overridden |
Indicates when the actual output controlled by this output is overridden by a user. |
False |
|
|
Output Position |
Provides the current Present Value of the output that this controller drives. |
0% |
|
|
Percent Cmd |
Indicated analog percent output used to control the single actuator providing heating or cooling. |
0% |
|
|
PID Tuning Reset |
Causes the PID objects to reset their tuning parameters to the default based on the appropriate Process ID. |
Normal Set Name: PID Tuning Reset |
|
|
Process Units |
Specifies the units for the PID. |
°C, °F Set Name: UNIT |
|
|
Process Variable |
When commanded to control cooling or heating, this variable is controlled and must respond to changes in the output. This is typically connected to the Zone Temperature. |
22 °C, 72 °F |
|
|
System Mode |
Control temperature. Either zone temperature, discharge air temperature, return air temperature or preheat temperature may be connected to this input. |
Auto Set Name: System Mode |