Module Use in Applications (Heating Staged Outputs) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Heating Staged Outputs Uses in Application System Selection Trees

Module Instance Name

Applications

Staged Heating Control v51

Fan Coil Application

Staged Supplemental Heating Control v51

To see a module's connections and how modules interact with it, view the Connections table.