Module Use in Applications (Heating Sequenced Valves with Low Limit) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Heating Sequenced Valves with Low Limit Uses in Application System Selection Trees

Module Instance Name

Applications

Sequenced Valves Preheat Control v50

AHU Mixed Air Single Duct Applications

AHU Mixed Air Dual Duct Applications

AHU 100% Outdoor Air Single Duct Applications

AHU 100% Outdoor Air Dual Duct Applications

AHU Multizone (Mixed Air Dual Duct) Applications

Sequenced Valves Reheat Control v50

All Air Handling Unit Applications

To see a module's connections and how modules interact with it, view the Connections table.