Module Use in Applications (Heating Proportional Valve with Low Limit) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Heating Proportional Valve with Low Limit Uses in Application System Selection Trees

Module Instance Name

Applications

Heating Zone X Output v51 (Where X Is 1-8)

Central Heating Applications

Proportional Valve Preheat Control v51

All Air Handling Unit Applications

Proportional Valve Reheat Control v51

All Air Handling Unit Applications

To see a module's connections and how modules interact with it, view the Connections table.