The application System Selection trees use the individual modules in this group using the names in the following table.
|
Module Instance Name |
Applications |
|---|---|
|
Heat Exchanger with Bypass Dampers |
|
|
Heat Recovery Wheel with Bypass Dampers v50 |
AHU Mixed Air Single Duct Applications AHU Mixed Air Dual Duct Applications AHU 100% Outdoor Air Single Duct Applications |
To see a module's connections and how modules interact with it, view the Connections table.