Attributes (Heat Recovery Glycol Loop) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following table describes the attributes used by the Heat Recovery Glycol Loop modules.

Table 1. Heat Recovery Glycol Loop Attributes

Name

Type 1

Description

Default Value

Compensator Heat Recovery Cmd

 

Controls the heat recovery valve. The valve is commanded from 0% to 100%. This output incorporates the Lead Compensator.

0.0

Display Units: %

Cooling Control Status

V

PID Status. The possible values are Normal, Overridden, Disabled, Low, Timing Low, High, and Timing High.

Normal

Set Name: Control Status

Cooling Mode

 

Desired cooling mode of operation.

Off

Set Name: AHU HR Cl EW

Heat Recovery OpenClose

V

Binary signal to the glycol valve.

Close

Set Name: Close/Open

Heat Recovery Percent Cmd

V

Analog signal to the glycol valve.

0%

Heat Recovery Suitability

 

Indicates if the heat recovery may be used for cooling control, heating control, or unsuitable for either control. The enumeration set is Heat, Cool, or None.

None

Set Name: AHU HR Suit

Heating Control Status

V

PID Status. The possible values are Normal, Overridden, Disabled, Low, Timing Low, High, and Timing High.

Normal

Set Name: Control Status

Heating Mode

 

Desired heating mode of operation.

Off

Set Name: AHU HR Ht GL

HR-OUTSTATE (State)

V, G

Indicates the current operational mode of the output controller.

Off

Low Limit Process Variable

 

Contains the low limit temperature process variable, normally connected to a sensor located in the exhaust duct after the Heat Recovery device.

4 °C, 39 °F

Low Limit Setpoint

 

Low limit temperature setpoint.

4 °C, 39 °F

Output Overridden

 

Indicates when the actual output that is controlled by this output controller is overridden by a user.

False

Output Position

 

Provides the current Present Value of the output that this controller drives.

0%

PID Tuning Reset

 

Causes the PID objects to reset their tuning parameters to the default based on the appropriate Process ID.

Normal

Set Name: PID Tuning Reset

Process ID

 
Specifies the type of process that this output controller is controlling when the mode is Tctrl:
  • Discharge Air Temperature (DA-T)
  • Zone Air Temperature (ZN-T)
  • Exhaust Air Temperature (ZN-T)
  • Zone Air Temp Compensated (ZN-T LC)

DA-T

Set Name: Process ID

Process Units

 

Specifies the units for the PID. For this particular module, °C and °F are the only two valid values.

°C, °F

Set Name: Unit

Process Variable

 

Contains the control temperature, and it may be connected to either Zone temperature, discharge air temperature, or exhaust air temperature. The latter signal is expected to come from a sensor in the exhaust duct upstream of the heat recovery device.

13 °C, 55 °F

Pump OnOff

V

Binary signal to the glycol circulating pump.

Off

Set Name: Off/On

Setpoint

 

Contains the desired setpoint for the process variable to be controlled to when the mode is Tctrl.

13 °C, 55 °F

1

C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)