Reliability (Cooling Proportional Valve with Dehumidification) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
All inputs use their last reliable value while unreliable.

If the outdoor air temperature is unreliable while in the Low OA Temperature mode, the module switches to the Limited Max mode as shown in Table 1.