Module Use in Applications (Fan VAV Series) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Fan VAVSeries Uses in Application System Selection Trees

Module Instance Name

Applications

Series Fan Control

VAV Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.