Attributes (Fan VAV Series) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The following table describes the attributes used by the Fan VAV Series modules.

Table 1. Fan VAV Series Attributes

Name

Type 1

Description

Default Value

Fan OnOff

 

Output command enumeration for information feedback representing the on/off status of the fan.

Set Name: Off/On

FAN-OUTSTATE (State)

 

Current operational state of the output controller.

Set Name: Off/On/Hold

Mode

 

Mode requested by State Selection.

Off

Set Name: Off/On/Hold

Percent Cmd

 

Contains the output for fan control (0-100%).

Display Units: %

Speed Setting

 

Contains the desired output (0-100%) when the fan is commanded on.

100.0%

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)