Module Use in Applications (Fan Three Speed) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Fan Three Speed Uses in Application System Selection Trees

Module Instance Name

Applications

Three Speed Fan Control

Fan Coil Applications

Heat Pump Applications

Unit Ventilator Applications

To see a module's connections and how modules interact with it, view the Connections table.