Fan Proportional - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This module controls a proportional fan. The module accepts as inputs a command, a heating percentage and a cooling percentage. Based upon the input command and parameter settings, the module outputs a percent command and an on/off command.

You can view and modify the modules in this group’s logic.