Primary States (Fan Single Speed) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
  • Off: Turn the fan off. The Fan OnOff is set to Off.

  • On: Turn the fan on. The Fan OnOff is set to On.

  • Hold: The fan remains in the state it was in when this mode was requested. If it is on, it stays on. If it is off, it stays off.