Reliability (Fan Relief Variable Capacity BSP Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
If building static pressure is unreliable, the fan state changes to off as shown in the Command Hierarchy table.

All other inputs use the last reliable value while unreliable.