Module Use in Applications (Dual Fan Run Together) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Dual Fan Run Together Uses in Application System Selection Tree

Module Instance Name

Applications

Dual Exhaust Fan Run Together

AHU 100% Outdoor Air Single Duct Applications

Dual Relief Fan Run Together

AHU Mixed Air Single Duct Applications

Dual Return Fan Run Together

AHU Mixed Air Single Duct Applications

Dual Supply Fan Run Together

AHU Mixed Air Single Duct Applications

AHU100% Outdoor Air Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.