The following table describes the attributes used by the Dual Fan Run Together modules.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Fan 1 Alarm |
This Enum input shows the current alarm status for the first fan. The input may be either Normal when there is proof of airflow or Alarm when there is no proof of airflow. |
Normal Set Name: Normal/Alarm |
|
|
Fan 2 Alarm |
This Enum input shows the current alarm status for the second fan. The input may be either Normal when there is proof of airflow or Alarm when there is no proof of airflow. |
Normal Set Name: Normal/Alarm |
|
|
Fan OnOff |
G |
This input is the fan command for the application. The activity uses this input to determine if a fan is needed to be commanded on or off. |
Off Set Name: Off/On |
|
Fan Percent Cmd |
Input defines the speed required for the fan or fans that are running. |
0.0 Display Units: none |
|
|
Fan 1 OnOff |
This Enum output is the fan command for the first fan. |
Off Set Name: Off/On |
|
|
Fan 2 OnOff |
This Enum output is the fan command for the second fan. |
Off Set Name: Off/On |
|
|
Fan 1 Output |
This Float output is the fan speed command for the first fan. |
0.0 Display Units: none |
|
|
Fan 2 Output |
This Float output is the fan speed command for the second fan. |
0.0 Display Units: none |