Dual Fan Run Together - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This module is designed to start and stop two fans so the fans run together, where both fans are commanded on and run during normal operation. For an air handler application two outputs control the speed of the fans. The module monitors the alarm status of each fan to determine whether the command must be commanded off. This module is implemented as a control activity.

You can view and modify the modules in this group’s logic.