Dual Pump Sequencer - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Dual Pump Sequencer module provides a Control System with dual pump control. This module is designed to control two pumps and to provide Lead Lag operation based on availability or runtime. The Dual Pump Sequencer module can only exist within a Control Sequence or Control Activity within a Control Sequence.