Attributes (Device OR) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following table describes the attributes used by these modules.

Table 1. Device OR Attributes

Name

Description

Default Value

Device 1 OnOff Indicates binary status of device 1. Off
Device 2 OnOff Indicates binary status of device 2. Off
Alarm OR If any input is on, this output is on. Off