Attributes (Damper and Fan Control) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The following table describes the attributes used by these modules.

Table 1. Damper and Fan Control

Name

Description

Default Value

Damper isAvailable Indicates the availability of the damper. True
Damper OpenClose Provides the control signal output to the damper BO. Close
Damper Status Indicates the status of the commanded damper. Open
Delay Indicates the time required to wait before starting the fan when the mode is On, and alternatively close the dampers when the mode is Off. 60.0 seconds
Fan OnOff Provides the control signal output to the fan BO. Off
Fan Status Indicates the status of the commanded fan. Off
Mode Indicates the required fan command. Off
State Represents the current state of the hybrid activity. Off