Primary States (Min OA Damper Proportional Output) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
  • Close: This command closes the minimum OA damper.

  • Open: This command opens the minimum OA damper.

  • Emergency Open: This command opens the minimum OA damper. While in this mode of operation, the low limit reset factor is ignored.

  • Min OA: The minimum OA damper is opened to its minimum position when commanded to this mode.

  • Ramp Min OA: The minimum OA damper ramps to its minimum position when commanded to this mode of operation.

  • Ramp Closed: The minimum OA damper ramps to closed when commanded to this mode of operation.