Module Use in Applications (Damper Minimum Position Controlled by OA Flow) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Damper Minimum Position Controlled by OA Flow Uses in Application System Selection Trees

Module Instance Name

Applications

Damper Min Reset by OA Flow v50

AHU Mixed Air Single Duct Applications

AHU Mixed Air Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.