Module Use in Applications (Damper Control for Volume Matching) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Damper Control for Volume Matching Uses in Application System Selection Trees

Module Instance Name

Applications

Proportional EA Damper Control for Volume Matching v50

AHU Mixed Air Single Duct Applications

AHU Mixed Air Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.