VF Primary Min Flow Control - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This module controls a proportional source within a control application. The module accepts a mode, a process variable, and a setpoint as inputs. Based upon the input mode and parameter settings, the module outputs a percent command and control status. This module resets the PIDs to default tuning parameters if the Reset PID Tuning input is true. This module is implemented as a standard Control Activity.

You can view and modify the modules in this group’s logic.