VF Primary Min Flow Control - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This module controls a proportional source within a control application. The module accepts a mode, a process variable, and a setpoint as inputs. Based upon the input mode and parameter settings, the module outputs a percent command and control status. This module resets the PIDs to default tuning parameters if the Reset PID Tuning input is true. This module is implemented as a standard Control Activity.

You can view and modify the modules in this group’s logic.