Module Use in Applications (Sequenced Output) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Sequenced Output Uses in Application System Selection Trees

Module Instance Name

Applications

HX1 Multi Valve Span

Central Heating Applications

HX2 Multi Valve Span

Central Heating Applications

To see a module's connections and how modules interact with it, view the Connections table.