The following table describes the attributes used by the Sequenced Output modules:
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Input (Float) |
Provides the variable that comes from the PID that is spanned across two outputs. |
0% |
|
|
Valve 1 Percent Capacity |
Indicates the capacity of the first valve, in percent. |
33.3% |
|
|
Valve 1 Percent Cmd |
V |
Provides an output from the span. |
0% |
|
Valve 2 Percent Cmd |
V |
Provides an output from the span. |
0% |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)