Module Use in Applications (Rotation Small) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Rotation Small Uses in Application System Selection Trees

Module Instance Name

Applications

Boiler Rotation Small

Central Heating Applications

Chiller Rotation Small

Central Cooling Applications

Cooling Tower Speed 1 Selector

Central Cooling with Optimization Applications

Cooling Tower Speed 2 Selector

Central Cooling with Optimization Applications

Cooling Tower Speed 3 Selector

Central Cooling with Optimization Applications

CW Pump Rotation Small

Central Cooling Applications

Primary CHW Pump Rotation Small

Central Cooling Applications

Primary Pump Rotation Small

Central Heating Applications

Secondary CHW Pump Rotation Small

Central Cooling Applications

Secondary Hot Water Pump Rotation Small

Central Heating Applications

Tower Rotation Small

Central Cooling Applications

To see a module's connections and how modules interact with it, view the Connections table.