The following table describes the attributes used by the Pump Startup Determination modules:
|
Attribute |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Device nn Status |
Indicates whether any of the pumps should be turned on. This module has 8 inputs. |
False |
|
|
Output |
G |
Indicates that one or more pumps should start. The output is an Or function of the inputs. |
False |
1 B - BACnet Exposed Parameter, C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)