Pump Startup Determination - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Pump Startup Determination module monitors the Chiller Selector and determines whether the pumping subsystems should be enabled. This module prevents variable speed headered pumps from activating until the Chiller Selector has opened at least one isolation valve. The Pump Startup Determination module has eight Boolean inputs and a single Boolean output. This module is only needed for variable speed headered primary pumps because the Chiller Selector and the Pump Selector are decoupled from one another.

Figure 1. Pump Startup Determination