Module Use in Applications (Pump Selector) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Pump Selector Uses in Application System Selection Trees

Module Instance Name

Applications

CWP Selector XX (Where XX Is 01-08)

Central Cooling with Optimization Applications

PCHWP Selector XX (Where XX Is 01-08)

Central Cooling with Optimization Applications

Pump Selector XX (Where XX Is 01-08)

Central Cooling with Optimization Applications

SCHWP Selector XX (Where XX Is 01-08)

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.