Pump Output Control - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Pump Output Control module provides proper operation of a constant speed or variable speed pump. It provides the on/off signal to turn on both variable speed and constant speed pumps. This module also provides the variable output signal for a variable speed pump. Based on the Mode input, it sets the Device OnOff output and the Percent Command Output. This module is implemented as a hybrid control activity.

You can view and modify the modules in this group’s logic.