Plant Control - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This module is responsible for controlling a central plant device (for example, a Boiler, Chiller, or Tower Fan). This module accepts as inputs a mode, command, on delay, safety, interlock status, interlock off delay, alarm delay, percent command, ramp time, percent limit, and maintenance switch. Based on the input command and attribute settings, the module outputs a rotate enable, device onoff, alarm command, interlock device command, and an output.

You can view and modify the modules in this group’s logic.