Damper Command OR - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Damper Command OR module provides the ability to OR the inputs to the module and passes the result to the output. This module is implemented as a control activity.

Figure 1. Damper Command OR