Cooling Tower Speed Count Determination - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Cooling Tower Speed Count Determination module determines the number of fans and the speeds at which the fans operate. This fan count can be used to start and stop cooling tower fans.

You can view and modify the modules in this group’s logic.