Module Use in Applications (Chiller Selector) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Chiller Selector Uses in Application System Selection Trees

Module Instance Name

Applications

Chiller Selector X (Where X Is 1-8)

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.