Module Use in Applications (Chiller Output Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection Trees use the individual modules in this group using the names in the following table.

Table 1. Chiller Output Control Uses in Application System Selection Trees

Module Instance Name

Application

ChlrX Control (Where X Is 1 to 8)

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.