The following table describes the attributes used by the Chiller Control modules:
|
Name |
Type 1 |
Description |
Default Valve |
|---|---|---|---|
|
Isolation Valve Command |
This Input is a Boolean command that opens or closes the two position isolation valve. |
False |
|
|
Stroke Time |
This input is the time (in minutes) for the module to drive the analog isolation valve command from zero to one hundred percent. |
1.0 Second |
|
|
Chiller Command |
Indicates the desired chiller operation. True means on and False means off. |
False |
|
|
Chiller OnOff |
V |
This output drives the chiller BO. |
Off Set Name: Off/On; Set Members: 0=Off, 1=On |
|
Iso Valve OpenClose |
V |
This output drives the two position isolation valve BO. Both the condenser water and chilled water isolation valves can be connected to this output. |
Close Set Name: Close/Open; Set Members: 0=Close, 1=Open |
|
Iso Vlv Pct Cmd |
V |
This output is the command for an analog isolation valve. Both the condenser water and chilled water isolation valves can be connected to this output. |
0.0 % |