Block Protect - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Block Protect module protects motor equipment by commanding the device to run periodically. The user-adjustable Max Off Time input determines the duration between run commands. If the Command input remains Off for a period greater than the Max Off Time, this module sets the State output to Run. The device remains in the run state for a period of time equal to the Blocking On Time input.

Note: The Block Protect module does not work correctly in Simulation mode. For example, when tested with 10X Simulation speed up, the Total Off Time must accumulate 10 times the Max Off Time before the State output transitions to the Protect state. This functionality will be fixed in a future release. This module does behave correctly in real-time Commissioning mode.

You cannot view and modify modules in this group’s logic.