Primary States (Slave Supply Flow Setpoint Control Dual Duct) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
  • Min: Output the Deck Min Flow.

  • Max: Output the Deck Max Flow.

  • Hold: Maintain the current flow setpoint.

  • Control: Adjust the flow setpoint to maintain the process variable at the setpoint.

  • Failsoft: Output the flow setpoint that is spanned between the Deck Min Flow and Deck Max Flow by the value of the Failsoft Value (percent).