The application System Selection trees in the software use the individual modules in this group using the name in the following table.
|
Module Instance Name |
Applications |
|---|---|
|
Supply Flow Setpoint Control v51 |
Note: The Flow Setpoint (VAV Single Duct) module instance appears in the Output Control category; however, to add a new Flow Setpoint (VAV Single Duct) module from the palette (Module Selection dialog box), select New from the State Generation header right-click menu.
To see a module's connections and how modules interact with it, view the Connections table.