Primary States (Flow Setpoint [VAV Dual Duct]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
  • Min: Output the Deck Min Flow.

  • Max: Output the Deck Max Flow.

  • Hold: Maintain the current flow setpoint. If the Output Overridden is true, then the Output Position input is passed to the Flow Percent.

  • Control: Adjust the flow setpoint to maintain the process variable at the setpoint. If the input PID Tuning Reset is not Normal, the Reset Tuning input to the PID is set to true causing the PID to recalculate its tuning parameters.

  • Failsoft: Output the flow setpoint that is spanned between the Deck Min Flow and Deck Max Flow by the value of Failsoft Value (percent).